You connect to an Enterprise Server or Enterprise Central so that you can set the servers to reset mode.
To set an Enterprise Server or Enterprise Central to reset mode you must run Device Administrator as an administrator. Refer to Windows how to run a program as an administrator.
Device Administrator must run on the same computer as Enterprise Server or Enterprise Central.
In Device Administrator, click Servers and then click Add server.
In the EBO server type list, select Enterprise Server or Enterprise Central.
Enter something in the Password box. The server is added even with an incorrect password.
Click OK.