earth_america
user_standard Log on
action_search_stroke
earth_america
Log on to rate and give feedback 1 2 3 4 5 Log on to rate
4
Concept

Concept


Products: All EcoStruxure BMS Products
Functionalities: Basic Functionality
Product version: 1.8, 1.9, 2.0, 2.1, 3.0, 3.1, 3.2, 3.3, 2022, 2023, 2024, 7.0, 7.1
2/5/2026

Safety Information

arrow1_rotation Important Information arrow1_rotation Please Note arrow1_rotation General Cybersecurity Information arrow1_rotation Safety Precautions

Important Information

Read these instructions carefully and look at the equipment to become familiar with the device before trying to install, operate, service or maintain it. The following special messages may appear throughout this bulletin or on the equipment to warn of potential hazards or to call attention to information that clarifies or simplifies a procedure.

 
action_zoom_plus_stroke

The addition of this symbol to a “Danger” or “Warning” safety label indicates that an electrical hazard exists which will result in personal injury if the instructions are not followed.

 
action_zoom_plus_stroke

This is the safety alert symbol. It is used to alert you to potential personal injury hazards. Obey all safety messages that follow this symbol to avoid possible injury or death.

Danger Danger

DANGER indicates a hazardous situation which, if not avoided, will result in death or serious injury.

Warning Warning

WARNING indicates a hazardous situation which, if not avoided, could result in death or serious injury.

Caution Caution

CAUTION indicates a hazardous situation which, if not avoided, could result in minor or moderate injury.

Notice Notice

NOTICE is used to address practices not related to physical injury.

Please Note

Electrical equipment should be installed, operated, serviced, and maintained only by qualified personnel. No responsibility is assumed by Schneider Electric for any consequences arising out of the use of this material.

A qualified person is one who has skills and knowledge related to the construction, installation, and operation of electrical equipment and has received safety training to recognize and avoid the hazards involved.

General Cybersecurity Information

Warning Warning

POTENTIAL COMPROMISE OF SYSTEM AVAILABILITY, INTEGRITY, AND CONFIDENTIALITY

Use cybersecurity best practices to help prevent unauthorized access to the software.

Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.

In recent years, the growing number of networked machines and production plants has seen a corresponding increase in the potential for cyber threats, such as unauthorized access, data breaches, and operational disruptions. You must, therefore, consider all possible cybersecurity measures to help protect assets and systems against such threats.

To help keep your Schneider Electric products secure and protected, it is in your best interest to implement the cybersecurity best practices as described in the Cybersecurity Best Practices document.

Schneider Electric provides additional information and assistance:

Safety Precautions

During installation or use of this software, pay attention to all safety messages that occur in the software and that are included in the documentation. The following safety messages apply to this software in its entirety.

Warning Warning

UNINTENDED EQUIPMENT OPERATION

  • Do not use the software or devices for critical control or protection applications where human or equipment safety relies on the operation of the control action.

  • Do not use the software to control time-critical functions.

  • Do not use the software to control remote equipment without proper access control and status feedback.

Failure to follow these instructions can result in death or serious injury, or equipment damage.

Warning Warning

INACCURATE DATA RESULTS

  • Do not incorrectly configure the software or the devices.

  • Do not base your maintenance or service actions solely on messages and information displayed by the software.

  • Do not rely solely on software messages and reports to determine if the system is functioning correctly or meeting all applicable standards and requirements.

  • Consider the implications of unanticipated transmission delays or failures of communications links.

Failure to follow these instructions can result in death, serious injury, equipment damage, or permanent loss of data.

Controller and server programming

It is important to verify that application programs are working as expected before downloading the application programs to the controllers and servers. When the application programs are downloaded, verify that they are downloaded correctly by verifying that the system operates as expected. This applies to initial system installations, system upgrades, and changes in an operational system.

Warning Warning

UNINTENDED EQUIPMENT OPERATION

  • Always verify that an application program is working as expected for all targeted servers, controllers, associated equipment, and entire system before downloading the application program to the controller or server.

  • Always verify that changes to an application program that runs in an operational system are working as expected for all targeted servers, controllers, associated equipment, and entire system before downloading the application program to the controller or server.

  • Always verify that the application program is downloaded correctly by verifying that all targeted servers, controllers, associated equipment, and entire system operate as expected after the application program is downloaded.

Failure to follow these instructions can result in death, serious injury, or equipment damage.